Export Data Log

From the Data Logger view, you can export a data log from the AC Source application to CSV (comma-separated values) format. You can export a data log even if the AC Sourceis currently acquiring measurements.

By default, exported files are stored in the "Documents" folder on your computer and are organized by instrument type. For example, C:\Users\<user_name>\Documents\Keysight\PathWaveACSource\Exports\.

 

To export the data log, click > Export Datalog. Set the Export Settings according to your preference and click Export.

Below are the Export Settings dialog details:

Export File Details

File Name - The default file name has a "Trace" prefix followed by a numeric index. For example, Trace 0. To change the default name, click on the existing name and edit it.

Export Path - The currently selected path for saving the file on your computer. To change the path, click Browse and browse to a different path.

File Type - The export file format is CSV (comma-separated values) format only.

Trace Data Summary

Number of Traces - The number of traces in the data file.

Total Samples - The number of samples in the data file.

Export Options

Column Separator - Select Comma (,) (default), Semicolon (;), or Tab as the column separator.

Record Range - Select to export all records (All Records), export records within the markers (Export using marker range), or export a range of records (Filtered by record number). If you select Filtered by record number, enter the Set to Start and Set to End record numbers in the fields.

See Also

Export Screen Shot

Load Offline Data Log